Part Number: SN65HVD1474
Other Parts Discussed in Thread: SN65HVD1477, , THVD2450, THVD1429
Hi all
My customer has below question, please comment and clarify.
Thank you and best regards
Ueli
------------------------------------
We are using SN65HVD1474 and SN65HVD1477 to drive 10m twisted pair cable.
It is one to one, unidirectional link.
Apparently 1477 (50Mbps) chip works worse than 1474 (20Mbps) for the same data rate of 20Mbps.
Would this two chips require different termination because difference in differential driver output?
What are the best termination methods for transmitter and receiver to active longest cable reach.
Is there any difference in input circuit between 1474 and 1477?
For example noise filtering or else?
Is there better driver for 20 Mbps application?