Part Number: TCA9554
Hello,
I have a question about TCA9554 address input pins(A0/A1/A2).
Are those inputs recognized only in power up sequence or any time?
Thanks in advance.
S.Sawamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9554
Hello,
I have a question about TCA9554 address input pins(A0/A1/A2).
Are those inputs recognized only in power up sequence or any time?
Thanks in advance.
S.Sawamoto
Hi Sawamoto-san,
The behavior I think you are referring to is called Dynamic Addressing. This feature describes a device's ability to change its address while powered without the need for a reset. The digital cores for TCA9554's family of devices supports this feature and means that the address pins are not latched during startup. Changes in these inputs can be changed any time without device reset. Note it is not recommended to change the state of these pins during the address phase of an I2C message.
Regards,
Eric