This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: DS90UB936-Q1 AC capacitor rating

Part Number: DS90UB936-Q1

Hi Team,

I have a question about DS90UB936-Q1 AC capacitors voltage rating.

Datasheet recommends to use 50 WV 0402 AC coupling caps on RIN0/1. However, it is difficult for customers to find these within required temperature ranges. Would it be okay if 16V-rated capacitor is used?

Should customer mostly take care about effective capacitance due to voltage de-rating (to check if 16V-rated capacitance does not de-rate under ~2.75V operatig voltage at FPD Link inputs)? 

Piotr