Part Number: DP83867IR
Hi all.
Hi.
The DP83867 datasheet contains a small section on layout, but leaves many questions unanswered.
I've read a lot of the posts on this forum about layout rules, and I have a question that I would like to ask about layout between the PHY and the magnetics. Specifically, about length matching.
1) As I understand it, the most critical rule is to match the lengths of the 2 signals in a pair. I can't find any TI recommended maximum mismatch. Is there one?
2) From reading the 802.3 spec, section 40.1.3.2, the receivers are independent of each other, and so each pair's length is somewhat independent of each other? Is the clock recovery system duplicated on each receiver in the DP83867?
40.1.3.2 Physical Medium Attachment (PMA) sublayer
...
The PMA Receive function comprises four independent receivers for five-level pulse-amplitude modulated signals on each of the four pairs BI_DA, BI_DB, BI_DC, and BI_DD,"