Part Number: SN65176B
TI,
Pertaining to the SN65176B differntial output, what happens to the opposite line when A (HI) or B (LO) is grounded? If B is shorted to ground does the output of A double it's amplitude so the differential voltage across B to A looks the same as if B was not shorted to ground. For example, if grounded B to A would be 0V to 5V instead of -2.5V to +2.5V like it normally should be from B to A? Or does A still come out to be +2.5V with reference to ground and B is 0V with reference to ground? Thank you for your help.