Part Number: TFP410
What is the power consumption per power pin section:
DVdd
PVdd
TVdd
Especially Tvdd.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TFP410
What is the power consumption per power pin section:
DVdd
PVdd
TVdd
Especially Tvdd.
Hi Victor,
Below are the maximum currents I saw across temperature in the characterization data at 165 MHz and worst case pattern:
DVdd: 54.23 mA
PVdd: 129.03 mA
TVdd: 79.94 mA
Regards,
I.K.
Hi,
Thanks for the information.
Are you sure about this?
It seems to me that given the functions of the pins that PVdd, being just the PLL, should have
the lowest current draw, and it only has one pin. And yet you show it has the highest
Hi Victor,
Yes, I'm sure. There are 4 reports that show the same correlation.
Regards,
I.K.