Part Number: DS90UB960-Q1
Hi team,
Our customer is using DS90UB960-Q1 and he asked a question to CSI-2 Forwarding of that device. Please support to answer his questions.
The display size is 1280x720, 4ch sensors input, all sensors are set VC-ID=0.
1) In the case, is the output display size 5120(=1280x4) x 720?
2) When one of sensors is disconnected, is the output display size 5120 x 720, or 3840 x 720?
3) When two of sensors are disconnected, is the output display size 5120 x 720, or 2560 x 720?
4) When three of sensors are disconnected, is the output display size 5120 x 720, or 1280 x 720?
Regards,
Nishimura