Part Number: TUSB320
Hi, I've implemented a TUSB320 for Type-C charger detection in our product. We are acting as the sink, but I've tried acting as a DRP as well. I can detect the ports on my laptop correctly in both high and medium current mode, as well as regular USB ports.
However, when using a phone charger (namely this one https://store.google.com/au/product/usb_c_18w_power_adapter_2 ), I fail to detect that a charger is even connected. When I measure the voltages, VBus is low, one CC line is low and the other is around 2.5V.
Are there any configuration steps that might cause or fix this sort of problem? I don't see any configuration options that would cause this.