Part Number: TCAN1048V-Q1
Other Parts Discussed in Thread: AWR1843,
Hi Experts,
Could you please let me know about Vol (max) when Io is smaller 1mA?
According to the datasheet, Vol (max) is 0.2*VIO when Io=2mA.
If VIO = 3.3V, Vol is 0.66V (max).
I plan to connect ti to AWR1843 which Vil = 0.62V at 3.3V.
If Io=2mA, TCAN1048V-Q1 might not drive AWR1843 Vil LOW.
I believe that if Io is smaller than 1mA, Vol(max) should be close to 0.1 * VIO which sufficiently drive AWR1843 Vil LOW.
Thank you for your kind check.
Best regards,
Hitoshi