Part Number: THVD1429
Hello team,
I'd like to confirm about the differential driver outputs(A&B) behavior during power down for THVD1429,
When Vcc and DE are turned off at the same timing. I expect a case that the same device is on the receiver side as well and only the power supply on the driver side is turned off, is there any potential issue or is there a recommended power down sequence?
From the datasheet, A&B should be HIZ when DE is low but I wonder a case of turning off Vcc.
Thanks in advance.
S.Sawamoto