Part Number: DS90UB948-Q1
Hi,
In our design, we are using LVDS to FDP (DS90UB947) and DSI to FPD (DS90UB941). Rather than design 2 different display modules, we are trying to implement a single display that will work with either FPD output.
The issue is that different AC decoupling capacitors are specified for each of the serializers (we are using coax connection with both).
DS90UB947: DOUT+ is 33nF and DOUT- is 15nF
DS90UB941: DOUT+ is 100nF and DOUT- is 47nF
So for the DS90UB948 deserializer to to be compatible with either serializer, what value AC decoupling capacitor can I use on the deserializer FPD input signals as I am assuming this should be matched on both ends of the FPD connection.
Or can I use the same values on the 2 serializers? Say 100nF and 47nF for both and the same values at the deserializer end?
Regards,
Peter