Part Number: DS100MB203
I have a DS100MB203EVK board, trying to read/write to the device on I2C bus. Can you help check what slave address I should use? According to Chapter 7.6 in the datasheet (http://www.ti.com/lit/ds/symlink/ds100mb203.pdf), slave address should be 0xB0 if AD[3:0] set to 0000'b. Can you provide 7-bit address explicitly starting with MSB and where AD[3:0] is located in this 7-bit address?
Thanks
Joe