Part Number: TCAN4550
Hi - I want to add a CAN interface to a MSP430 , but also want to have a 3V3 bus voltage as well as Io voltage- is there anythign available?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
By 3.3-V bus voltage, do you mean this is the pull-up voltage for CANH? If so, may I ask why would you want this? There are 3.3-V powered discrete transceivers available, but these are typically used in applications where a 5-V supply is not available (while the lower-voltage transceivers maintain compatibility with 5-V devices, they often cannot meet ISO 11898-2 physical layer requirements across all operating conditions). Since the TCAN4550 integrates a 5-V LDO, though, rail availability wouldn't be a concern.
Regards,
Max