Part Number: TCAN1042DEVM
hello,
Kindly assist me in configuring the TCAN1042evm for my project.
1. I wish to configure this module with VIo as input for VRXD.
2. Do I need to give a supply to VRXD (3.3V - 5V)
3. with the following configuration, I find the value of VRXD to be decaying, I guess because of the capacitor discharging when I see in multimeter, from 3.3v to 0v.
4. In datasheet it is mentioned, to add C6 capacitor. Can you tell what changes do I have to do if I'm using VIO.