Part Number: TPS65986
Other Parts Discussed in Thread: TPS65982
This part is now LTB status. Is there a drop in replacement?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65986
Other Parts Discussed in Thread: TPS65982
This part is now LTB status. Is there a drop in replacement?
Hi,
We will get back to you soon.
While you could switch over to the TPS65982ABZBHR for a drop-in device, our recommendation is that you move to the TPS65987DDHRSHR for the latest PD3.0 compliant device from TI.
Regards,
Karl Fleischmann
Actually, these do not appear to be equivalent. Pins A5, A9, B5, B6, B9, K4, and L4 look different. Can you please verify?
Thanks,
Lauren
Hi Lauren,
When using the TPS65982 as a TPS65986, please follow the pin-out guidelines of the TPS65986 as the additional pin functionality of the TPS65982 is not used when operating as a TPS65986.
Regards,
Karl
Hi Karl,
I think I'm happy with your answer above, but please can you just confirm that in the case of using the TPS65982 as a drop in replacement, we should ignore the pin specification for the TPS65982 where it actually contradicts the TPS65986 datasheet?
For example, pins A5 and B5 (a second I2C interface on the TPS65982) are GND for the TPS65986, but the TPS65982 datasheet says of these pins: "Tie pin to LDO_3V3 or VDDIO (depending on configuration) through a 10-kΩ resistance when used or unused." So can you please confirm that leaving these pins connected to GND is indeed acceptable for the drop in replacement?
Many thanks,
Jon
Hi Prajith,
Thank you for confirming. I will also assume that pin L4 can safely be treated as a direct connection to ground. (The datasheet for the TPS65982 describes L4 as an input, with a recommended 1k-5M to ground if unused.)
Thanks,
Jon
Hi Jonathan,
I wanted to ask another question on this. Should the current configuration for software for the TPS65986 work okay for the replacement TPS65982? Is there anything the customer should be aware of or looking to change? Will the configuration work fine if they are not using the functions on the 7 new pins?
Thanks,
Lauren
Hi Lauren,
I'm just another customer here - but I second your question!
+1 from me.
Thanks,
Jon
Hi Lauren,
The TPS65986 configuration can run directly on the TPS65982 silicon no changes needed to the configuration file.
Regards,
Karl