Part Number: TUSB3410
Hello,
I download sllc428b (tusb3410_driver_v6.7.4.0_setup) and get it installed on my PC which is WINDOWS 10 Pro, 64bits.
I installed in Admin mode.
There is no VCP created and the communication program I'm using (Aurora Installer) says the driver is not installed and there is no port available.
Note: I was using the TUSB3410 with PC working Windows XP qnd Windows Seven without issues. I had to switch to W10 as Windows updates for Seven stopped recently.
Could you help?