Part Number: DP83TC811R-Q1
Other Parts Discussed in Thread: DP83TC811
Please see the attached filesPhy initialization problem111.docx
I have a PHY initialization issue.
I’m using DP83TC811R Texas Instruments Physical Layer Transceiver.
I configured the EN and WAKE pins as outputs and set them to logic 1 (The Phy should be enabled).
I generated a negative pulse to RST pin. (RST pin is set to logic 1 final state)
When I set the EN pin to 1 logic and read the INH input I can see its logic 0 (Phy is Enabled).
From datasheet of DP83TC811R:
There is a 25Mhz crystal that is connected to XI and XO. For some reason there is no frequency on
this crystal.
Can this be the reason the PHY initialization fails?
Please Advise.Phy initialization problem111.docx