Part Number: DP83TC811S-Q1
Other Parts Discussed in Thread: DP83TC811EVM, DP83822I, , DP83TC811
Hello,
I am using the DP83TC811S-Q1 in a purely physical ethernet to automotive ethernet media conversion application. I followed the reference design for the 811 chip (DP83TC811EVM) and decided to use RGMII with the DP83822I ethernet PHY. Prior to implementing the design, I tested the EVM by using 2 in a back-to-back configuration (PC1 <-> EVM <-> EVM <-> PC2) and I used iperf3 to monitor packet loss. In this scenario, the EVM worked fine and I recorded near 100Mbps with 0% loss. After designing the media converter and getting the boards, I tried a similar test (PC1 <-> my converter <-> EVM <-> PC2) using iperf3 and I recorded around 1.2% loss going from PC1 to PC2, and 0% loss going from PC2 to PC1. I don't believe there are any issues with the EVM as I had tested it beforehand, so I'm thinking that there might be an issue with the transmitter in the 811, or the receiver in the 822 on my board. I used 2.49k pull-up resistors on the Rx_D1 and Rx_D2 pins so that MAC[2:0] = 110 to get the 811 PHY into RGMII with internal Tx and Rx delay mode. On the 822 chip, I used a 13k pull-up and 2k pull-down on the CRS pin to get it into mode 2, and a 6.19k pull-up and 2k pull-down on the Rx_ER pin to get it into mode 3.
Are there any issues with this configuration? I figured these were the same pull-ups/-downs populated on the EVM board as well.
Thanks,
Tharindu