Part Number: LMH0397
Other Parts Discussed in Thread: SIGCONARCHITECT,
Hi,
MODE_SEL is pulled down to VSS with 1kΩ resistor, ENABLE is pulled up to VIN(2.5V) with 1kΩ resistor and SCL and SDA are pulled up to 3.3V with 4.7kΩ resistors.
So, is there any condition that video data cannot be detected and video isn't output when the above input terminals are fixed?
If yes, please give me the details of the conditions.
Best regards,
Kato