Part Number: TCAN1042HV
Hi there,
we're using a TCAN1042HVDRB on one of our design because we need to stand 65V on CANH/CANL.
Unfortunately, it seems that the transceiver fails at 60V.
We've bought the chips on Digikey and we're not sure that the chip is really the "H" suffix (even if the reference is good on the bag) since the marking is the same (1042V).
Could you please confirm that this transceiver can stands 65V on CANH/CANL without external component on the bus ?
Best regards,
Maxime.