Part Number: TPS65987D
Hi all,
We have the following use case: ApolloLake SOC and TPS65987D for using in DRD mode. The USB-HS signals routed directly to ApolloLake from USB-C
Our idea is to start Linux from USB stick in production case. I mean in case, when the board contains not programmed SPI-NOR for TPS65987D. Is it possible? If yes, then some other questions to it
As I see the TPS65987D has the default configuration 2
for probably our case
And as I understand we can select the configuration 2 via combination of resistors on ADCIN1 but what should we do with the SPI_MISO? We have now the pullUp on this pin as it is defined i datasheet.
For Usb_Vbus_Detect we wanna use the GPIO14 event and for Usb_OTG_ID the GPIO13 event. Should we implement any pullUps/pullDowns to get the feature for our case running? Will that pullUps/pullDowns not disturb the functionality of TPS65987D when the SPI-NOR not yet flashed and in case when it is already flashed?
Thanks,
Best Regards,
Sergey