Part Number: DS90UB960-Q1
Team,
We plan to run multiple (up to four) FPD links back into the DS90UB960. We’re mostly interested in the following for this part:
- The datasheet’s table #53 seems to indicate that any of the four FPD link streams can be forwarded to either MIPI port 0 or MIPI port 1. Can you confirm that we can use this part as a 4:2 hub? We would want to run both MIPI outputs and switch which FPD link streams get routed to each MIPI output.
- How to configure it for synchronous mode with a 24 MHz clock generated to the DS90UB953 parts we will have downstream?
For reference, we plan to pair this with a DS90UB953ATRHBTQ1 for our serializer. We are running it with a MIPI camera, 2-lane CSI-2 at 1080p, 30 fps
Thank you.