Part Number: XIO2001
Hi team,
Could you please answer to the below questions?
Q1
Is the function of XIO2001 only register management?
In other words, does PCIe / PCI R / W the register of XIO2001, and does XIO2001 output the processing as it is as a PCI / PCIe signal?
Q2
Does the following recognition match the waiting time for PCI detection?
The waiting time for PCI detection is managed by the Secondary Latency Timer Register (described in data sheet p50)
> This read / write register specifies the secondary bus latency timer for the bridge, in units of PCI clock cycles.
⇒ "secondary bus latency timer" indicates the waiting time for PCI device detection.
Q3
Regarding the determination of the PCI CLK frequency, do you agree with the following recognition?
The PCI CLK frequency is set by HW.
Pull-up / down is connected to the M66EN pin and the PCLK66_SEL pin, and the corresponding value is determined from 25, 33, 50, and 66 MHz. (See data sheet p117)