Part Number: DP83867IS
Customer has a few questions regarding the DP83867IS:
1. Customer is changing PHY IO voltage from 1.8V to 3.3V. Will the crystal drive circuit be affected by the different IO voltage at all? We’re guessing not, but figured we’d double check just in case. Is it good practice to get our crystal re-tested with this change or can we say with confidence there will not be any change in the crystal drive circuit?
2. We might also have a possible situation coming up where we could have two sets of magnetics on the same signal path/board for the PHYs. Are there any glaring concerns at the operability of this situation? I think we’ll run it through a compliance test to see what we find but if there are any thoughts or specific things to look for in this situation that would be good to know.
3. It could also be possible to have the opposite scenario occur. Other than isolation/ESD issues, are there any other concerns with having no magnetics in the signal path between two PHYs at all?
Please advise.
Thanks,
Mark