Hello TI-Community,
i am searching for a LVDS Driver & Receiver Pair that is 3V - 5V power and logic (TTL) compatible.
is there any device that fulfills this?
or must i decide if i want 3V or 5V Logic and power levels?
my target application is
- single-way (Master to slave only)
- 2-wire SPI (clock + data)
- >10..30 Meter twisted pair cable
- sometimes i have 3.3V and sometimes 5V logic
- driver: 3.3V..5V power and TTL logic output
- receiver: 3.3V..5V power and TTL logic output
- in some configurations this means level shifting is achieved
i have had a look at
but did not find any matching part..
thanks for any hints or information how to find this :-)
sunny greetings
stefan