This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO3130: Support two port at same time

Part Number: XIO3130

Hi Sirs,

Sorry to bother you .

We would like to check does XIO3130 could meet our application?

Our function block as below, we need two channels operate at the same time to transmit data. (such like PCIE hub)

If no does TI have others solution can share?

Thanks!!

Function block:

  • Hello-

    The application you referenced in the block diagram requires PCIe Gen-3 switch.  The XIO3130 is a PCIe Gen-1 1:3 switch.   There is also a need for a PCIe Gen-3 to 2.5G bridge.  TI does not offer such a solution.

    Regards,

    Davor