Part Number: DP83TC811R-Q1
Hi,
We want to use 2 DP83TC811R-Q1 chips to send and receive RGMII data. We have configured one of them as master and one of them as slave. We are also setting the 0x0017 register accordingly so that RGMII mode is selected with internal delay disabled (Register settings 0x4245). We are receiving the RGMII data correctly but with RX error asserted continuously. We are receiving ESD_ERR, even though we are making sure Tx_err is never made high during transmission. Are there any settings which we have missed ??