Other Parts Discussed in Thread: SN65HVD234, TCAN334, SN65HVD234-Q1
Hi All,
In our product we need a CAN trx and we have inserted the TI SN65HVD234D trx.
The first question is: is the component compatible with CAN FD? Actually I would need to understand if the tranceiver, unless the maximum working speed, is transparent from the point of view of the CAN protocol?
I should also add the device wake-up feature from CAN (activity only and not by specific message).
I evaluated other trx, but I did not find a 3.3V wake-up component. There would be the possibility to keep the SN65HVD234D component in stand-by mode, taking advantage of the message received. The problem arises from the current in stand-by mode, which can reach 600uA: I need to stay below 100uA.
I am also evaluating the identification of can trx via discrete, do you have any application notes or schematics to obtain this functionality?
Many Thanks,
Antonio