Part Number: TUSB1310A
To whom it may concern,
I recently purchased a hitech global FMC USB development board which I'm interfacing with a Cyclone 10 GX development board via the FMC connector. The hitech global FMC USB board has a two TI TUSB1310A chips on it but unfortunately, I'm only able to partially interface with one of the two USB 3.0 transceiver chips. The ULPI side of the chip I'm able to interface with could not be fully mapped via the FMC connector so, I'm not able to exercise the USB 2.0 (ULPI) functionality. Since I'm really not interested in the USB 2.0 functionality, I'm fine with that. However, four of the ULPI data pins are also part of the strapping option pins (namely ULPI data bits 4,5,6 and 7), if ULPI data bit 7 is left floating, can that cause the transceiver to remain in isolation mode and not be able to receive or transmit data packets at all?
Regards,
Luis