Part Number: DP83849C
Hi,
Maybe you are able to reference Case CS0132290 solution as well.
The issue I have is I would like to identify connections between qty 2 RJ45 connectors and the DP83849C as well as the connections between the DP83849C and a SMT32F407 micro. I realize that the SMT part is not a TI but I have no choice in the micro as it is what my customer wants. I could attached a drawing of the connections. I will list them here as to what they are
MII_TX_CLK, MII_TX_EN, MII_TXD(3:0), MII_CRS, MII_COL, MII_RX_CLK, MII_RXD(3:0), MII_RX_DV, MII_RX_ER, MDIO, MDC
These signals are form the Ethernet interface solutions for the STM32F407 application block diagrams.
If the TI device selected is not suitable maybe advise one that would be.
Maybe you are unable to help but would appreciate a response or if you do have information.
Thanks in advance,
Ron