Part Number: DS90UB934-Q1
Hi team,
I have some quick questions from customer. Below is the interface of their processor, it has only 8 data inputs. 934 has 12 data outputs, can I use 8 outputs and leave the other 4 not connected? From my understanding, it is OK but I still have some questions to confirm with you regarding to this application.
1. Which mode should I configure in 934, RAW10, RAW12 or both OK?
2. If RAW10 mode is enabled, should I use ROUT0-7 or ROUT2-9 or both OK?
3. When connecting 934 with 8 data outputs to the processor, it cannot pair with 953 in DVP mode, right? Only when connecting 10 or 12 outputs can it support 953, right?
4. Any other points should be pay attention when using only 8 outputs? Thanks for your help!
Best Regards,
Arie