Part Number: PCA9544A
Can't find information about electrical connection to thermal pad (VQFN).
Can I connect it to ground ? Should I ?
Best regards
Adam Górski
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9544A
Can't find information about electrical connection to thermal pad (VQFN).
Can I connect it to ground ? Should I ?
Best regards
Adam Górski
Hey Adam,
You can connect the thermal pad to GND if you would like. This device is typically not used with large currents (our Ron is also low) so the power dissipation is low, meaning you wouldn't expect it to heat up much. Leaving it unconnected is also okay to do.
Thanks,
-Bobby
Hey Bobby,
That was question more about internal electrical connection than thermal flow.
Can you confirm that thermal pad is not connected internally ( electricall meaning ) or internal connections allows to connect it to ground ?
Please confirm and I will close my issue as resolved.
Best regards
Adam Górski