Part Number: DP83630
Dear Sir, please answer
I use DP83630 & PIC32MX microcontroller. I use MII interface. I used quartz crystal 25 MHz connected to X1, X2 inputs of the DP83630. I'd like to replace quartz crystal with the external generator 25 MHz (connected to X1 input of the DP83630).
QUESTION: Is it necessary to make changes to the PIC32MX microcontroller program code in connection with this replacement? The fact is that, the program code for the PIC32MX was written long ago and I would not want to change it.
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by