Part Number: PCA9306
Hi Team,
I using I2C Level shifters from TI PCA9306DQER .
The Topology that I using is attached.
Is it ok to connect PCA9306 in parallel as attached topology?
Thanks,
Shlomi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCA9306
Hi Team,
I using I2C Level shifters from TI PCA9306DQER .
The Topology that I using is attached.
Is it ok to connect PCA9306 in parallel as attached topology?
Thanks,
Shlomi
Hi Shlomi,
Yes, it is alright to use PCA9306 in parallel connections as depicted in your attachment. Please note that PCA9306 does not buffer the I2C bus so the effective capacitance for the bus is the summation of all buses (1.2V, 1.8V, and 3.3V buses). Pull-up resistors will have to be sized appropriately.
Regards,
Eric