Part Number: DS90UB941AS-Q1
Hi,
I wanna make the IRQ system using SER-941 and DES-948.
In SER-941, I already connects GPIO0 and GPIO1 to the IRQ input of HOST SoC.
and I received the IRQ of Slave IC (DES Side) w/ D_GPIO(18 pin) in DES-948.
at this situation,
- Can I connect the IRQ of Slave IC from DES-948 (D_GPIO input) to SER-941 (GPIO0 or GPIO1 output) ?
- If it could be done, How can I connect and what is the register related ?
Thanks.