Part Number: TUSB9261
Hi,
Can I use the part TUSB9261 to convert SATA signal to USB signals?
Regards,
Shafeeq
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261
Hi,
Can I use the part TUSB9261 to convert SATA signal to USB signals?
Regards,
Shafeeq
Hi Malik,
Is there any other solution from TI which can be used for this function?
Regards,
Shafeeq
Hi Malik,
Could you please explain awhat 's the typical application for converting SATA signal to USB signals?
The device is called USB to SATA bridge. Does that mean the device convert USB signals to SATA signals?
And form datasheet application : PC with USB port -TUSB9261-HDD with SATA port, I assum that the bridge is bidirectional signals communication. Thanks.
Best Regards,
Tess Chen
Hi Tess,
The electrical signals are bidirectional however on the USB side there are additional protocol requirements that prohibit this application. In short, converting SATA to USB implies that you want TUSB9261 to act as a DFP or USB Host. TUSB9261 is only intended to be used as a USB device or UFP then converting to SATA.