Part Number: TPS65987D
Hey,
A customer I am supporting is attempting to use the tps65987D as a sink , and I had some questions:
- Is there any internal flash or non-volatile memory that can hold configuration settings? Basically can you program it once and never program it again? If no, are there any default configuration settings currently loaded on the device that don't need the use of an external processor?
- They are using the device to negotiate power with a type-c host as well as transfer data. However, they also want to be able to deliver power when the device is connected to a dummy host (i.e. a type-c wall adapter). Can the tps65987d simply pass power when no type-c host is present? How is this typically done?
- Is minimum power negotiable when connected to a type-c host? (i.e. don't send me less than x watts)
Regards