Part Number: TUSB9261
Hi Experts,
Our customer is using our TUSB9261 to make the design, and they used below SPI Flash W25Q32JVSSIQ. After they programmed the firmware with a SPI Flash programmer, TUSB9261 can not detect the mSATA hard disk. But if they changed back to our EVM Flash, their board works fine. So can you help to check if the attached SPI Flash is compatible with our device or not?
Thanks.