My TYPE-C PORT can be used as UFP or DFP.
If using TUSB1064, can the USB signal of TUSB1064 be switched between DFP and UFP?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My TYPE-C PORT can be used as UFP or DFP.
If using TUSB1064, can the USB signal of TUSB1064 be switched between DFP and UFP?
thanks.
Hi,
TUSB1064 is intended to be used on the sink side of Type-C with DP Alt-mode application. The device is used for UFP_D pin assignments C, D, and E from the VESA DisplayPort Alt Mode on USB Type-C Standard. From a USB prospective the data role (DFP or UFP) does not impact TUSB1064.