This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF230: Retimer's profile file(.exe) of SigCon Architect EVM GUI

Part Number: DS250DF230
Other Parts Discussed in Thread: DS250DF210, DS250DF410, DS250DF810, DS280DF810

1) Hi, where can I download the DS250DF230 Retimer's profile file(.exe) of SigCon Architect EVM GUI?

2) Is the profile of DS250DF230 the same as DS250DF210?

  • Hi Frank,

    1). Please send me email with your company email address and we can provide access to the DS250DF230 design documents including updater and other documents. Here is email address: nasser.mohammadi@ti.com

    2). Please note temperature lock range is different between these two products. DS250DF230 is more geared toward wireless back haul and has higher temperature lock range(~150 degC).

    Regards,, nasser

  • Hi Nasser, Rodrigo,

    Thank you, and I still have questions about register value setting in programming guide,

    For DS250DF230, When using external 25MHz (NOT 30.72MHz) oscillator clock,

    1) Table 23 & Table 24 are NOT applicable for DS250DF230 using 25MHz, right?

        Can I still utilize Reg_0x2F for standard rate setting for DS250DF230 using 25MHz, how and which table?

    2) If I set both Reg_0x2F & Register 0x60, 0x61, 0x62, 0x63 values with different rate/sub-rate, which register(s) will take effect/prioritize?

    3) Should I calculate the Reg_0x60 - Reg_0x63 value through the formula (6)-(11) in programming guide section 7.7.1?

    Or can I also use SigCon GUI & updater.exe to input the rate & tolerance to let GUI to generate the registers value automatically?

    Or both 2 methods work?

     

    7.6 Standard Data Rate Settings
    The DS2x0DFxx0 channels must each be preprogrammed for the expected data rate(s) to ensure CDR
    lock. Users can program the rate/sub-rate to one of a set of pre-defined standard values to quickly
    configure the DS2x0DFxx0. The rate/sub-rate settings are programmed by writing to channel
    Reg_0x2F[7:4].
    Table 23. DS280DF810, DS250DF810, DS250DF410, DS250DF210 Standard Rate Modes
    Configurable from Reg_0x2F

    STANDARD RATE SETTING

    REG_0x2F VALUE
    [HEX]

    REG_0x2F WRITE MASK
    [HEX]

    10.3125 Gbps

    00

    F0

    10.9375 Gbps

    10

    12.5 Gbps

    20

    RESERVED

    30

    25.0 Gbps

    40

    25.78125 Gbps (default)

    50

    RESERVED

    60

    28.125 Gbps

    70
    (DS280DF810 only)


    Table 24. DS250DF230 Beta Version Standard Rate Modes Configurable from Reg_0x2F(1)

    STANDARD RATE
    SETTING

    REG_0x2F VALUE
    [HEX]

    REG_0x2F WRITE MASK
    [HEX]

    RECOVERED CLOCK FREQUENCY
    [MHZ]

    12.16512 Gbps

    00

    F0

    30.72

    9.83040 Gbps

    10

    30.72

    10.13760 Gbps

    20

    30.72

    24.33024 Gbps

    30

    30.72

    4.91520 Gbps

    40

    30.72

    25.78125 Gbps(Default)

    50

    32.2265625

    10.31250 Gbps

    60

    32.2265625

    25.78125 Gbps

    32.2265625

    10.31250 Gbps

    70

    32.2265625

    6.14400 Gbps

    80

    30.72

    (1) This table is valid only when the calibration clock is 30.72-MHZ

    7.7 Manual Data Rate Configuration

    7.7.1 25-MHz Calibration Clock
    The procedure for calculating the register 0x60, 0x61, 0x62, 0x63 values when the calibration clock is 25
    MHz is as follows:

    REG_0x60_val = Floor{(DataRate * 1024) / (64 * 25E6)} & 0x00FF, For DataRate > 13E9 bps

    (6)

    REG_0x60_val = Floor{(DataRate * 1024) / (32 * 25E6)} & 0x00FF, For DataRate ≤ 13E9 bps

    (7)

    REG_0x61_val = Floor{(DataRate * 1024) / (64 * 25E6)} & 0xFF00 >> 8 | 0x80, For DataRate > 13E9 bps

    (8)

    REG_0x61_val = Floor{(DataRate * 1024) / (32 * 25E6)} & 0xFF00 >> 8 | 0x80, For DataRate ≤ 13E9 bps

    (9)

    REG_0x62_val = Reg_0x60_val

    (10)

    REG_0x63_val = Reg_0x61_val

    (11)


    For reference, Table 25 shows the register values for manually programming a few standard data rates.

    Table 25. Register Settings for Common Data Rates using 25-MHz Calibration Clock

    DATA RATE

    REG_0x60 VALUE
    [HEX]

    REG_0x61 VALUE
    [HEX]

    REG_0x62 VALUE
    [HEX]

    REG_0x63 VALUE
    [HEX]

    REG_0x18[6:4]
    VALUE
    [HEX]

    25.78125 Gbps(1)

    74

    C0

    74

    C0

    0

    25.0 Gbps(1)

    80

    BE

    80

    BE

    0

    20.625 Gbps

    90

    B3

    90

    B3

    0

    12.5 Gbps(1)

    80

    BE

    80

    BE

    1

    10.3125 Gbps(1)

    90

    B3

    90

    B3

    1

    (1) These rates can also be configured by selecting the appropriate rate setting in Reg_0x2F.

  • Hi Frank,

    Please note Rodrigo has already responded to this question through the email you had sent him.

    Regards,, Nasser