Part Number: TUSB2046B
Other Parts Discussed in Thread: TPS2547, , TUSB4041I, TPS22914
I need a 4 port hub with 1.5A charging downstream ports. I've located the TUSB2046B and TPS2547. Once I noticed that the logic for the TUSB2046B PWRON is inverted from the TPS2547 EN, I became concerned if these are a good fit for each other. Is there a better combination of devices for my application? Or, do I just need to simply add an inverter between the two devices?
Thanks!
Tony