Part Number: DP83867IR
Hi team
Customer would like to make RX_DV/RX_CTRL Mode3 for Gigabit ethernet. In current their design, Pull-up resistor = 5.6kOhm, Pull-down resistor = 2.4kOhm.
And they observed that the link is established when the partner(FPGA) is powered-on, while the link is not established when the partner(FPGA) is not powered-on.
Is this correct behavior?
I think their resistors value can violate +/- 1% tolerance of the recommended resistors, Pull-up resistor = 5.76kOhm, Pull-down resistor = 2.49kOhm.
So if the voltage of RX_DV/RX_CTRL-pin is out of target voltage, what kinds of things may happen?
Regards,
Noriyuki Takahashi