Part Number: TUSB2077A
Hi,
I am designing a 7 port USB Hub with TUSB2077A USB Hub controller,
anyone who can help to double check it ? thanks a lot !
BR,
Vincent.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB2077A
Hi,
I am designing a 7 port USB Hub with TUSB2077A USB Hub controller,
anyone who can help to double check it ? thanks a lot !
BR,
Vincent.
we are reviewing the schematic and will give feedback soon
Vincent;
couple of questions here:
1: for crystal you need to connect both pin 44 and 45.
2: For BUSPWR, you need to pull high to 3.3v, not 5v
3: it seems you designed a ganged self powered system, where do you get Vcc5?
Hi, Brian,
Thanks a lot, I would like to use 48MHz oscillator,Which ones need attention?
This Hub controller is one of onboard devices, carrier board has 5V power source,
In addition to the above question, are there any error in schematic ?
BR,
Vincent.
it's fine to use 48Mhz oscillator.
For power supply, you use DVcc3.3 for device supply and DVcc3.3 is from Vcc3.3. and some of the pin is pullup to Vcc3.3, there could be power sequence issue. All those control pins need to pull up DVcc3.3?