Part Number: TUSB8041
Other Parts Discussed in Thread: TPS2561
Hi
The design page (page 33) in the data sheet of the controller depicts the interfacing of TPS2561 (a power distribution switch) with the controller.While in the page 3 topic titled "Description (Continued)" paragraph 2 states
" An individually port power controlled hub switches power on or off to each downstream port as requested by the
USB host. Also when an individually port power controlled hub senses an over-current event, only power to the
affected downstream port will be switched off "
So,if I provide the supply (5V @ 500mA per port (Since I WANT IT IN USB 2.0)) externally do I need to use TPS2561.If so why? SINCE it is said that "when an individually port power controlled hub senses an over-current event, only power to the affected downstream port will be switched off" - this is the same functionality I need
How should I configure the pins OVERCURxz & PWRCTLx/BATENx .Where do these route to if there is no power distribution ICor should there be one?
Does the controller has the over current protection or are the pins OVERCURxz only for sensing.