Part Number: TCA8418E-EVM
Other Parts Discussed in Thread: MSP-EXP430G2ET, TCA8418E, MSP430G2553, TCA8418, MSP430FR6989
Hi,
I am running Eval board p/n TCA8418E-EVM with MSP-EXP430G2ET. After finding the right drivers, I was successful in using TCA8418E_Flasher.bat to program the supplied text file.
BUT, when launching setup.exe in TCA8418E-EVM GUI folder, I am getting "Could not detect COM PORT."
Any idea?
Thanks,
(PS:
I am using Windows 10 pro
For completeness, below is result of running the batch file, TCA8418E_Flasher.bat )
"
* Warning: Found device does not match -n selection:
- Selected: MSP430G2553
- Found: MSP430G2xx3
- Continue? (Y/N): y
* Loading file into device...done
* Verifying memory (TCA8418E.txt)...done
*
* ----------------------------------------------------------------------------
* Arguments : -n MSP430G2553 -w TCA8418E.txt -v -g -z [VCC]
* ----------------------------------------------------------------------------
* Driver : loaded
* Dll Version : 31400000
* FwVersion : 31200000
* Interface : TIUSB
* HwVersion : E 6.0
* JTAG Mode : AUTO
* Device : MSP430G2xx3
* EEM : Level 1, ClockCntrl 1
* Erase Mode : ERASE_ALL
* Prog.File : TCA8418E.txt
* Verified : TRUE
* BSL Unlock : FALSE
* InfoA Access: FALSE
* VCC ON : 3000 mV
* ----------------------------------------------------------------------------
* Starting target code execution...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (No error)
* ----------------------------------------------------------------------------
*/
Press any key to continue . . .
"