With a coax connected, I2C Back Channel controlled '953 running and transferring data to a '954, can you update the '953 Device ID Register (Address 0x00) from the strapped default to a new value and set the SER_ID_OVERRIDE via the I2C BC control from the '954 and then update the '954 SER_ID (Address 0x5B) to match the newly updated '953 setting with the devices linked and running?
Are any other writes required to update the '953 I2C address while linked and running with I2C BC control from a '954?