Part Number: SN65HVD230
Dear All,
I want to interface STM32 nucleo 64 board to CAN Bus.
I developped a first application using TJA 1051 transceiver powered with 5V (CJMCU 1051) and it works fine.
Then I need to replace the nucleo board with another one with 3.3V power supply,
so I tried the SN65HVD230 transceiver (Arduino tecnoiot module ) instead of 1051, powered with 3.3V
Unfortunately I have no communication at all. I tried to add another 120 ohm resistor between CANH and CANL
and also the split connection with 4,7nF capacitor but i have nothing.
In front of the transceiver I use Vector CanCase with SJA1000 transceiver at 1Mbs-1
Any idea ?
Best Regards,
Patrick.