Part Number: TUSB8020B
Hi Team,
My customer would like to use TUSB8020B as a HUB that is connected to a SOC that has OTG function.
In Case 1(Normal using case), SOC is as host that can access to slave devices. This scenario should be no problem.
In Case 2(programming SOC), customer would like to use USB port to upgrade SOC code and in this situation the SOC side becomes a slave and device side is connected to PC as a host, and device 2(DN 1) is connected with a device. Does this user scenario workable? If not, is there any advice can be shared with customer?
Thanks very much.
Vincent Chen