This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: DP83822I: LINK Issue

Part Number: DP83822I


Hi Nikhil-san

 

thank you for contacting.

 

How are you detecting 1.8V?

⇒See attached S / W configuration.

  0x0421 is read before setting 3.3V.

  

When not linking, I tried the following:

But it does not return.

Please tell me the cause.

 

・0x0000 bit9:  Autonego, reset

・0x001F bit14: Initializes all digital circuits except internal registers.

・0x001F bit15:

・0x0000 bit15:

・0x3000 bit15:

・0x041F   :3.3V setting

2311.PHY register.xlsx