Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65988, , TPS66020
Not having had the bandwidth yet to have read through and understand all of the TPS65987D & TPS65988 documentation, is it possible to make use of the IC as a simple on-off switch capable of handling bidirectional current flow of 5A at up to 20V? This is for a non-USB application with no CC signals, having no Type-C PD power negotiation. Are there "low level" control bits that would simply enable and disable the power path to turn on and off when commended to?